Part Number: TPSI3052-Q1
Other Parts Discussed in Thread: TPSI3052
Tool/software:
Hello,
We have the TPSI3052-Q1 designed into our product to drive a Mosfet in Three-wire mode. We have had a few instances where the the driver has failed with a short between VDDP and VSSP. Upon investigation, we observed that the VDDP voltage (referenced to VSSP) during operation ranges from 5.7V to 6.3V, which exceeds both the recommended operating conditions and the absolute maximum rating of 6.0V as specified in the datasheet. Additionally, we have captured distorted rising edges on VDDP during power-up, resembling switch bounce or ringing, which may be contributing to transient overvoltage conditions.
My question is, is the failure mode (VDDP–VSSP short) consistent with damage caused by exceeding the absolute maximum voltage rating and/or poor power-up signal integrity?
Driver circut below:
Thank you