This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25820: Optimized duty cycle

Part Number: BQ25820


Tool/software:

Hi,

I would like to verify/ confirm the DCDC duty cycle

Our case:

- Lithium ion battery pack, 5S or 6S *the PCBA will be modified between this two battery pack options, required minimal BOM change, meaning FB resistors only

- Charging levels- 30W up to 70W

- External VDC input power- 36Vdc (required for others requirements)

The calculated DCDC charger D.C is  50% to the 5S option and 60% for the 6S option,

what is yours opinion?

BR

Shachar