This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070: Maximum Duty Ratio

Part Number: TPS63070

Tool/software:

Hi team,

The PS pin is dropped to Lo and the switching frequency fs is set to fixed (2.4MHz) to output 5V.
I thought it would always be 2.4MHz, but when the potential difference between input and output is less than 0.8V, it becomes 1.2MHz.
I assumed that this was due to a limit on the maximum duty ratio or potential difference, is this correct?
And if so, I would like to know the specific value.

Best Regards,
Ryu.