Part Number: LMR36503-Q1
Other Parts Discussed in Thread: LMZ23605
Tool/software:
I am using LMR36503RS3QRPERQ1 IC.
The frequency was set to 400 kHz by attaching 41.2K Ohm to the RT pin.
I confirmed that the frequency was operating at 60~70 kHz, not 400 kHz, because the load connected behind the buck IC was small.
When designing a CLC filter with reference to AN-2162 document, which fs value should I use, 400 kHz or 60 kHz?
And how do I find the Vin-ripple-p2 value?
Can you elaborate on the process of calculating the 'Cfb' value in Example 1 (LMZ23605)?