Part Number: UCC5390
Other Parts Discussed in Thread: UCC5350, TVS0500
Tool/software:
Hi,
I'm using the UCC5390SC in a single-phase UPS application. One of the six gate drives used in the device is sometimes damaged during startup.
When the UCC5390SC is damaged, the resistances measured with a multimeter on the secondary side, between VCC2, VOUTH, VOUTL, and VEE2, are the same as those of a good IC. However, the resistances on the primary side, between VCC1 and GND1, show a resistance of 900 ohms on the damaged IC and infinity on a good IC. The current consumption of the VCC1 supply (5V) goes up to 26 mA on a damaged IC, while it is only 1.2 mA on a good IC.
What could be damaging the UCC5390?
Could a transient on the VCC2 side cause a failure on the VCC1 power line?
Ari.