Tool/software:
Peripheral Circuit for Forced PWM Mode
I want to use forced PWM mode with a 3.3V Fixed output.
The VSET/MODE pin
(1) Because I want a 3.3V output, it must be connected to GND via a 205kΩ resistor when the IC is powered on.
(2) However, because I want to use forced PWM mode, it must be set high.
→Is it okay to connect VSET/MODE pin to GND via a 205kΩ resistor and also to the VOUT pin?