Tool/software:
We have a design that we use the TPS63710 to convert +5VDC into -2.5VDC for a negative reference on an ADC. For 99% of our modules, it works fine, but there is an issue with the 1% where we get a fault from the PG pin that it has failed. I have checked the voltage input on the supply and its stays above the 2V and check the temperature of the part and it does not get hot. This leads me to Vout is not regulated during these instances. I'm starting to believe it's the DC Bias on Ccp capacitors but not sure. Can you review the schematic to see if there is any issues you see?