This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56837: Current Ripple w.r.t. Switching Frequency

Part Number: TPS56837

Tool/software:

Hi Team,

We are working with a high speed switching load which operates at 8V, The 8V Domain is supplied from a stable 24V Power domain.

While using a TPS56837RPAR Buck Converter, we observed peak currents of around 6A, This was observed with a switching frequency of 500kHz.

Upon experimenting with a Switching frequency of 800kHz by just changing the value of the resistor connected to MODE pin, We observed that the peak current in the 8V Domain reduced drastically to around 2A. We have observed that the mean current remains almost the same while the difference in peaks is drastic. We want to understand the effect of switching frequency on this high switching load. Please do let us know the relation b/w the switching frequency and output current ripple.

I have attached the schematics in our design and the observed peaks for your reference.

Switching Frequency 500KHz 800kHz
Peak Current 6A 1.85A
Mean Current 160.7mA 150.5mA
Observed Waveform