Tool/software:
Hi team,
Currently, the CPU is used as a single-phase power supply for the core power supply (VCCIN) of the CPU.
On top of that, we are considering the contents of changing the TDP50W CPU to TDP67W and 83W.
A comparison of the current consumption of the CPUs is shown below.
Based on these results, it appears that a single-phase supply is not feasible and a duplex supply is necessary.
Is there any solution?
Do I still need to use two?
If possible, I don't want to change the board and would like to be able to input with only one.
Best Regards,
Ryu.