Tool/software:
Dear Experts,
We are currently using BQ76200 and have discovered a phenomenon during testing. When we set CHG-EN, CP-EN, DSG-EN, PMON-EN, and PCHG-EN low, the measured output voltage of DSG is 0V, and the output voltage of CHG and PCHG to GND is 44V, which is approximately equal to the battery voltage. At this time, our Pack+, CHG, DSG, and PCHG peripherals do not have any external circuits; We also enabled DSG-EN, CHG-EN, PCHG-EN separately, and tested the driver output to GND voltage. The results are as follows. Currently, we do not know if this is a normal voltage? Hope to receive an answer, thank you