Tool/software:
Hi, Experts.
My custom board has built-in LP87334D, PMIC for AM243.

Referring to the circuit diagram in the data sheet (Using the LP8733xEVM and LP8732xEVM Evaluation Modules (Rev. A),
I worked on the circuit as follows.
It was soldered well by checking the position of pin 1, and 5V is also entering normally.
However, each output voltage pin has the following voltage output.
0v85 -> 0V
3.3V -> 0.625V
1.8V -> 0V
0v85 -> 0V
3.3V -> 0.625V
1.8V -> 0V
Best Regards,
+
The regulator is not enabled because the EN pin is not connected. Let me finish the question. Thank you.