Part Number: TPS25221
Other Parts Discussed in Thread: TPS2552D, TPS2552-1, TPS2552
Tool/software:
Hi Team,
Customer is seek a TPS25221 p2p part but with the enable is active low, could you help check if this is available?
Regards,
Will
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Will,
Do you need a P2P alternative that comes in a SOT-23 package? Or WSON?
BR,
Seong
Hello Will,
We do not have any other 6-pin USB power switch with adjustable current limit with max 2A continuous current. The next one down is the TPS2552D which is:
The next one down is the TPS2552 or TPS2552-1 (latch-off version), which is:
Hope this helps,
Seong