Tool/software:
Device: BQ40Z50-R5
Cells: 3S20P (Samsung 50E)
Hi, I need some advice regarding the learning cycle.
During the learning cycle, Qmax update is not occurring and the Update Status is stuck at 0x04.
The pack capacity is 98,000 mAh, so I calibrated the current scale to 1/3.
(For example: real current = 15 A, calibrated current = 5 A).
I also set the design capacity to 32,667 mAh.
Charge and discharge voltage range is 2.5 V ~ 4.2 V.
I will attach the log file from my learning cycle test.
Could you please review it and let me know what might be causing the issue?