Tool/software:
Hello — question about the TPS4813-Q1 precharge/LWU behavior (ref: Fig. 7-13 in the datasheet).
If the bypass FETs’ VGS (G2) reaches V_G2_GOOD while the precharge of the load capacitor is still ongoing, and the load current exceeds I_LWU, will the device switch to MAIN FET (G1) conduction immediately — potentially before precharge is complete — causing a large inrush? Or does the TPS4813 have an internal sequencing/lock that prevents handover until the precharge sequence is finished regardless of V_G2_GOOD/I_LWU?
If it can hand over early, what’s the recommended way to guarantee switching to G1 only after precharge is complete (internal setting, layout change, external comparator, timing, use of ILWU hysteresis, etc.)?