This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Problem with starting

Part Number: UCC28950


Tool/software:

Hello. I created prototype by this:

8372.webench_ucc28950_design_forum.pdf

It works, but with load above 1A there has been heating of diodes D17 and D18.

I set som delays, no effect. Last I try to decrease frequency from 150kHz to 100kHz with Rt resistor changing. From this time nothink works. No outputs, only Vref is 5V and EA+ is 2.5V. Put Rt resistor to before value, no effect. Checked all connections, everything. Disconnect trafo, uses only  Vbias, nothink.  I change device UCC28950 for new one, the same. Some days ago, when I start it first time, with Vbias above 8V, there was pulses from OUTA ... OUTD. Now nothink. Checked DCM, RSUM, CS, still no outpus. What can cause this? What minimum must be connected for OUTA..OUTD get pulses? I'm frustrated, whole day without real effect.