Other Parts Discussed in Thread: BQ25302
Tool/software:
Hello.
I'm designing solar charging using BQ25570 and USB connection circuits using BQ25302.
The LOAD I wanted to use exceeded 100mA, so I connected the load directly to the battery without using VOUT of BQ25570.
So I attached the Schottky diode to the VBAT pin of BQ25570 and the BAT pin of BQ25302 respectively and connected it to the battery. (See also circuitry)
If I use BQ25570 and BQ25302 at the same time, do I need to design the circuit like this? Or I'm asking if you have any recommendation circuit design tips to use solar charging and USB charging at the same time.
Regards,
JP