Tool/software:
Hi expert,
Can you help on below register configuration issue? Thanks!
1. The 3B register ADC_CONV and ADC_START were set to 1 during initialization, but the value of the 3B register address read back shows ADC_START set to 0 during program execution. Why is this?
2. After writing 0xFF to the 3A register and enabling ADC detection in the 3B register, with low power mode turned off, the current values read from registers 2B, 28, and 29 are all 0, regardless of whether the battery is connected or not. What could be the reason for this?
3. The voltage values read back for VBUS, VSYS, and VBAT do not match the actual voltage values. Does this need calibration? How can it be calibrated?
4. After setting the input voltage limit at 0A/0B, the system immediately shuts down. The actual set value is 13.6V, but the actual input is 12V. Why is this? How should it be set?