Tool/software:
Hello.
Our actual application is using the TPS723 in the following conditions:
1. Vin = -7V
2. Vout = -5V
3. Output load is 185mA
Pdiss should be ~0.37W
-
We understand that the output current should be less than 200mA. We realized that there is a protection circuit that limits the current ~300mA min (550mA typ).
We are wondering if we can increase the output current up to 300mA approx. We also consider the change of Vin to -5.5V (or around it) in order to reduce the LDO dissipation (should be less than in actual application).
What would be the drawback of doing it? Will it continue to regulate to -5V? Is it safe in all conditions?
Thank you in advance!