Other Parts Discussed in Thread: LMR60430, LMR51435, LMR51450
Tool/software:
Hi,
I have used TPSM63610RDFR DC DC Converter in one of my designs to generate 28V to 8.5V. But, now, I have a requirement for 28V to 26V conversion instead of 28V to 8.5V conversion. Since TPSM63610 only supports output voltage upto 20V, this cannot be used further in my design. So, for the same, kindly suggest any pin to pin footprint compatible DC DC converter (height restriction: 4mm), in place of TPSM63610 DC DC Buck convertor, which can meet my design requirements.
Also, please suggest EMI filters (IC), that can be used at the output of this DC DC Convertor to handle the switching noise.
Regards,
Sahil