This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSI3050-Q1: fails

Part Number: TPSI3050-Q1
Other Parts Discussed in Thread: TPSI3050,

Tool/software:

I use a TPSI3050 to enable a capacitor-discharge FET. This FET is preceded by a ~0.2A current limiting circuitry.

At higher voltages (~300V) this will lead to failures of TPSI3050. Resistance (as measured by DMM) between Pins VDDM und VSSS is ~11Ohms afterwards. 

Seemingly FETs are not destroyed and substitution of TPS3050 will repair ciruitry. 

TPSI3050 is used in 3-wire mode. Ub=4.7V, Rp=9K09

Currently I am running out of samples for repairing/troubleshooting the issue so any clue would be very welcome. 

Attached is a simplified schematic.