TPS65994AD: Motherboard with TPS65994AD Connected to Type-C Display - No Output After Hot Plug

Part Number: TPS65994AD
Other Parts Discussed in Thread: TPS65994,

Tool/software:

I am working on a mature ADL-P project using the TPS65994 as the PD controller. The Type-C port is configured in ONLY SINK and DFP modes. It connects to a daughterboard (acting as UFP and Source device), which hosts the display. The display signal is processed by the daughterboard’s PD controller before being transmitted to the motherboard. Currently, I am encountering an issue: during hot-plugging, the UFP device detects the HPD change, but the system does not respond. After unplugging the screen, the display parameters still remain in the system. When the screen is plugged back in, there is no output (the display parameters persist). The log is shown in the figure below.

Any suggestions for debugging this issue would be greatly appreciated!