This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150: LM3150:

Part Number: LM3150


Tool/software:

Hi there,

I use the LM 3150 to step down from 26V to 21.3 .

Input should be max. 2.3 A.

Its to charge a LiFePO Battery.

When i connect first the input at 26 V then the Battery its working.

If the Battery is connected first it will destroy the controller evry second or thirt time.

Can you help me to save the chip?

Its very urgent.

Thank you

Ingo