This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480: Regarding the CAD symbols

Part Number: LM7480
Other Parts Discussed in Thread: TPS1685, INA750B, TMP118

Tool/software:

Hi team,

My customer is preparing a prototype board to verify the operation of a power switching circuit using ideal diodes.
When creating the circuit, they are downloading CAD symbols for each device from TI.com.
However, the symbol creation fails when executing the batch file.

The Symbol IN seems to have completed successfully, so it appears to be working correctly, but the SMB file remains empty.
The error log indicates that licenses for "ftf" and "laf" are missing.

---------------------------------------------------------------------------

C:\zuken\CR8000\ul_LM74800QDRRRQ1\ZukenCR\ftf\ZukenCR.ftf.err
C:\zuken\CR8000\ul_LM74800QDRRRQ1\ZukenCR\laf\LM74801-Q1DRR\zdsain.err

---------------------------------------------------------------------------
In the customer's environment, only the schematic CAD license is available, and they do not have licenses for footprints or other features.
Does this mean that a full license environment is required to use this tool?

Would it be possible to receive just the SMB file?
The devices for which the SMB symbol is needed are listed below.

LM74800

TPS1685

TPS37044

INA750B

TMP118

Best regards,

Kyohei