This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR60410: The issue of chip usage

Part Number: LMR60410


Tool/software:

When using the LMR604103SRAKR DCDC, with an input of 5V and an output of 4.5V, when carrying a load of 1A, the output voltage is only 4V, and the voltage drop is relatively large. What is the reason for this? How should it be solved?

Below are the schematic diagram and the switch waveform. It seems that there is a problem with the switch waveform