This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700D-Q1: LM74700D + CSD18511 -> valid? and short circuit protection

Part Number: LM74700D-Q1


Tool/software:

hello,

i test the lm4700 and csd18511 for our configuration and design an prototype. everything works as excepted.

but this is my second try so i want to be sure that everything complied with.

We use the protection against battery short circuit, and it works :-)

i ve some notes:

  • the CS18511 rds on is below the recommendation 
  • voltages larger 20V i don't except
  • i except no reverse voltage, that is not the main purpose here
  • it is not necessary to protect the power supply against short circuit

I am wrong, or can i use the configuration?

Thanks

i ve attached an simplified schematic: