Other Parts Discussed in Thread: LM73606
Tool/software:
Hi TI,
I've been working on an inverting buck-boost converter utilising the TPS7H4010-SEP based on the application note SNVAA76 - Radiation Tolerant Inverting Buck-Boost Converter with
TPS7H4010-SEP. For my prototype boards I'm using the LM73606.
The configuration (seen below) is based on the 12V/-12V configuration from the application note, modifying it to operate as 15V/-15V.

Note: R5 is not populated, as well as the part list exclude parts.
Note that the UVLO from this design does not seem to work, I've rectified this issue already and R9 (the 10k) resistor is removed for now, pulling up the EN pin.
The Issues
In general I'd say there are currently two issues:
1. The switching frequency does not seem to correspond to the RT values. It appears to be variable depending on the load, rather than consistent.
2. The output voltage "drops" (because it's negative it actually increases, but you get the point) for increasing load.
Output Voltage vs Output Current
The first verification step was to simply plot output voltage for different load scenario's. I'm loading the circuit with a programmable load in constant resistance mode.

In experimentation, trying to figure out what's going on with the switching frequency I've noticed that if RT is left unconnected, the device appears to operate better, however there doesn't seem to be any significant change in actual switching frequency observed on the SW node.
Switching Node Measurements
In order to assess the issue I've performed measurements of the switching node SW (pin 1 of L1). It should be noted, that for these measurements the output voltage itself is actually quite stable (except the last one). Just not at the right value. I've looked at the plots of the 12V/-12V design in the application note and the behavior of this IBB design seems to not be the same. Debugging has proven difficult since a lot of the statements from the regular datasheet do not appear to be valid for this IBB configuration.
No Load - Output = 15.2 V.
See two measurements below of the same no load condition. The timing between pulses appears to fluctuate. I believe this makes sense since the device is operating in the auto mode, only switching when required. Note that purely looking at the square wave part of the switch, it appears that the "Switching frequency" is ~ 2Mhz here, whilst based on the RT setting (39k) it should be 1 Mhz.


1k Load - Output = 15.17 V
I take this as my baseline, this is a "light load" and behaviour seems to be what I'd expect from the auto mode.
50R Load - Output = 15.01 V
With a 50R load, the output voltage has already dropped to 15.01 V. The current here is ~ 300 mA. Looking at the switching node below I notice that even-though the output voltage has already dropped by 200 mV, the device still appears to idle for about 50% of the time. (my assumption is that that's what happens when those sine oscillations appear, perhaps their presence is my whole issue, but I haven't been able to find the reason for their existence) Furthermore, the switching frequency (looking purely at the square wave) appears to be ~ 1 Mhz here.

10R Load - Output = 14.4 V
Current here is ~ 1.4A. Here approximately 600 mV is dropped and the switching frequency appears to be 500 kHz, with still some "off time". Another observed effect is the short peak in the SW node whilst the node is at it's lowest point. Finally, there still seems to be some "non switching" time, eventhough the output voltage is nowhere near reached.

5R Load - Output = 9.22 V
This is where the device seems to completely lose it. This output voltage is no longer stable and the SW node seems to be a bit all over the place. I'm still intruiged by those "peaks" I noted earlier, my first thought is that there might be some internal overcurrent protection kicking in, but the hysteresis of that is in the order of 46 ms, which is far too long.

Additional Information
Some additional invo that may help:
1. The Inductor has a saturation current of 5.6A, which I believe may be part of the issue and I'll be trying to find a higher rated inductor.
2. I've tried to connect the RT resistor to GND instead of the output voltage, as well as using a potentiometer in it's place. With the RT to GND, the switching frequency seems completely unaffected, regardless of value. With the RT to the output voltage (N15V) at least it appears to do "something", but not what one would expect.