This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21750: UCC21750QDWQ1

Part Number: UCC21750


Tool/software:

Hi Team,
We need you support on selection of preferred current amplifier / driver part number for UCC21750QDWQ1. which is having 10A peak current. But out requirement is 20A. We wanted to used same Gate Driver along with some current amplifier or Buffer.

UCC21750QDWQ1---- 10A 
Current amplifier 20 A



Thank and Regards,
Abdul

  • Hi Abdul,

    There are isolated gate driver with 17A drive strength, will that be an option?

    We have the following EVM design which supports external buffer design, please refer it for the overall circuit design, the buffer component (different models) can be selected based on your voltage and current requirement. As it is not TI part, i am not recommending specific part for it.

    https://www.ti.com/lit/pdf/SLUUCK0

    Thanks

    Sasi