This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65135: VPOS output voltage tolerance

Part Number: TPS65135

Tool/software:

Hello,

Our customer has a question VOS output tolerance at VOS=6V/20mA load condition.

Due to the customer LCD panel specification, VPOS=6V, VNEG=-6V setting is mandaroty. Since TPS65135 VPOS can set up to 6V VPOS, he is worried about VPOS voltage becomes lower that the LCD panel spec of 5.9V min.

Could you please let us know VPOS voltage tolreance or variation in VPOS=6V setting , 20mA load current, Ta=-40 to 85C ?

Best regards,