Tool/software:
Hello support team,
We are design a board that can be supplied either from a USB PD source or a standard power source.
If the source is compatible with PD, then we intend to use TPS25751D to negotiate a 20V/5A profile.
If the source is just a standard power supply with no PD support, then the TPS25751D won't be able to negotiate anything. In that case we still wish to close its PP_HV switch if the voltage is in a correct range that we monitor by an other component. I took a look in the TPS25751 Technical Reference Manual but I couldn't find if it is possible to control PP_HV switch with I2C registers from MCU.
Could you please tell us if this is possible ? Otherwise we will just add electronics to bypass TPS25751D.
Best regards,
Adrien