This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455EVM-GUI-SW: Question about minimal bridge setup

Part Number: BQ76PL455EVM-GUI-SW


Tool/software:

I have looked at the bridge sample for this ic and it uses a step up regulator to create a 12V from which it powers the ic via the internal regulator / external transistor LDO. The datasheet tells me that this chip can also be powered by supplying power to the VDIG ( and VIO) pins, while sidabling the internal regulator via device configure CMD 0x0E.  For a minimal briidge configuration, this looks promissing. I wont be measuring anything on the voltage pins, i will only be using htis chip to let a cpu communicate to a string of other BQ76PL455's that are daisy chained to it.   Am i missing somting? why is the bridge sample using a step up regulator for this purpose. Would i be violating/ breaking anything if i woul d to power the chip directly to VDIG, disabling the internal regulator and connecting all sence pins to ground..?  That would be really minimalistic. 

  • Jeroen,

    We do not recommend using these devices in any new projects. The newer line of BQ796xx devices are safer and more accurate. 

    You can do what you are suggesting. 

    Regards,

    Bo

  • I need to interface with (legacy) devices that already have this chip in them and because the inter-chip communication is proprietary i don't have a lot of choice.  If you know a newer model chip that can interfacein a daisy chain  to this older model then i would be very interested.

    Thanks for confirming that i can power the chip via an external power,connect the battery 'sence' pins to ground and only use the chip for upstream communication. A kind of uart-to-iso-spi (?) bridge so to say. 

  • Hi Bo,

    i tried powering the device with just 5V on the DIG and the TOP / SENSE pins to ground or 5V but i get no response from the chip. Only with 12V on the TOP pin, it comes to live. Is there any way i can make this work with just 5V and no step up ?  Feels silly to only use the step up to make the sense pins happy..

    Cheers

    Jeroen