Tool/software:
Dear TI team,
I was looking through the TPS7A4501-SP data sheet and noticed Vadj is stated as 1.174V minimum, 1.246V maximum across the full operating range. I assume this then scales linearly so that for a design with Vout=3.3V for example the variation in Vadj could lead to an output of anywhere from 3.202V (1.174*3.3/1.21) to 3.398V (1.246*3.3/1.21), i.e. +/- 98mV deviation from nominal.
Is this assumption correct? Looking at the value stated for 25°C only gives a +/- 14mV variation in Vadj from typical, is it right to assume this is device-to-device variation with the additional 22mV variation for the full range being due to temperature?
Kind Regards,
David Court