This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A94: Inquiry on Input Voltage Derating for TPS7A94

Part Number: TPS7A94

Tool/software:

Hi,

Attached is the schematic. My requirement is to regulate 5.3 V down to 5 V. The datasheet specifies an input voltage range of 1.7 V to 5.7 V, but it does not provide a derating curve for input voltage.

Could you please clarify how to account for derating of the input voltage in this case?

  • Hey Misba,

    There is no specific input voltage derating for this LDO. As long as you operate within the recommended input voltage range provided in the datasheet (in this case, 1.7 V to 5.7 V), the regulator is expected to function normally.

    The only limitation would be thermals caused by heat dissipation but there's no risk at your specified conditions.

    Thanks,

    Vahnroy