This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546D24S: Output Voltage Setting error

Part Number: TPS546D24S

Tool/software:

Hello,
We have Built 40Amps single phase PCB's which have 4 IC(TPS546D24S)  in each PCB, After Configurations while power conversion without load output of some of the ICs were showing around 6.5V.

We have Checked the feedback Resistance between vosns and Vout, and Gosns and GND i.e 49.9 ohm.
We have Checked voltage across capacitor between vosns and gosns i.e same as output voltage 6.5V
And also checked the Output at SW pin of IC , below is the images of the SW pin output

Above image referring the output voltage of 6.5v where the set voltage was 0.55V  (SW_OUTPUT AT 6.5V)


SW_OUTPUT FOR WORKING IC AT 0.55V

Attached the schematic for reference
EPU40X4_6LAYER_1.pdf

Thanks for any help in advance
Thanks and Regards,
Nagendra