Tool/software:
I have a uC circuit powered with a fixed 3.3V voltage. However during programming i want to supply the circuit with the programming adapter, which might deliver output voltages with slightly more than 3.3V (up to 3.5V). How would the TPS62162 behave when I connect this voltage to its output pin?
When supplying an output voltage it will travel over the body diode of the FET connecting SW and VIN and switching on EN. However, when FB>3.3V the SW-VIN FET should turn off (however there is still the body diode conducting) and the FET connecting SW-PGND might turn on.
My concern is that when the FET is switched on it drives enough current to GND to destroy either my programming device or the TPS62162.
So my question: Will the FET connecting SW to PGND turn on when I connect an output Voltage to the regulator output which is higher than its set value.