TPS62A03: ENABLE min/max values in "6.5 Electrical Characteristics"

Part Number: TPS62A03

Tool/software:

Hello,

On the datasheet "6.5 Electrical Characteristics" under "ENABLE"

Are the values of the "EN high-level input voltage" and "EN low-level input voltage" in the incorrect "MIN" & "MAX" locations ?

Is the "EN high-level input voltage" 0.8V minimum and the "EN low-level input voltage" 0.4V maximum ?

Thanks

  • Hello,

    In fact it is not wrong, it is probably the way you interpret this description.

    For any voltage >0.8V, the EN pin will definitely be driven HIGH.

    For any voltage <0.4V, the EN pin will definitely be driven LOW.

    For voltages in between there is a chance of false read-outs by the device.

    I hope this helps!

    BR, Febin