Other Parts Discussed in Thread: TPSI3050
Tool/software:
Hello Team,
We are using the IC TPSI3050 in one of our products.
Attached is the schematic of the same.
Can you please review the same?.
The device is working in 2-wire mode.
The VSSP is connected to the CGND (Ground of the power supply).
The signal IN_H4 is a 12V signal and is completely isolated from the CGND.
Our device consists of almost 300 such signals.
For testing these devices, we have made a test jig
In the test jig, we have given a 5V at the IN_H4 pin of the device.
This 5V is taken from an AC-DC power adapter.
The GND at the DC side (5V side) is connected to the Earth pin at the AC side.
Our device is supplied with a 12V AC to DC adapter and the CGND (GND at the +12V side) is also connected to the AC earth.
So ultimately, both the signals at either side of the TPSI3050 is referring to the same GND.
What behavior can we expect in this situation?.
is there any problem if there is no isolation between the supplied at VSSP or VVDP and VSSS.
Looking for your reply