This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ-BATTERY-PROGRAMMER-SW: Run time Error 339 "Component 'MsComCtl.ocx' or one of its dependencies not correclty registered: a file is missing or invalid

Part Number: BQ-BATTERY-PROGRAMMER-SW
Other Parts Discussed in Thread: BQ30Z55

Tool/software:

 Hello,
I am trying to install the “bq Evaluation Software.” I have tried it on several computers. I started with a WIN10, then a WIN7 system, and finally a WIN XP 32-bit system. Always with the same result. “Runtime Error 339; msComctl.ocx” is missing or not registered correctly. The error message also appears when I have added the file to /Windows/System32 and registered it. 
Could it be a problem with the software? Unfortunately, I cannot use EvalutionStudio because it does not support BQ30Z55 chips.
I bought a Phantom 4 with two batteries. These are discharged below the voltage threshold because the previous owner left them unused for too long. Technically, the batteries are still fine. 
Can anyone help me?

Translated with DeepL.com (free version)