TPSM843820: Design tool for WEBENCH or CALC-TOOL-TPSM843X20

Part Number: TPSM843820

Tool/software:

Dear Sirs and Madams,

We would like to know about inductance when considering current limiting and inductor ripple current.

Our operating conditions are as follows:

Vin: 5V

Vout: 1.8V

Fsw: 1MHz

WEBENCH does not generate any errors under these conditions.

However using CALC-TOOL-TPSM843X20, a warning or caution will be issued regarding inductor ripple current.  

Our application does not allow switching frequencies above 1MHz.

This module uses a 220nH inductor, so the inductor ripple current is calculated to be approximately 5.2A (= approximately 65% ​​of the output current).

Naturally, I understand that inductor ripple current affects ⊿Vout, current limit, and responsiveness.

Is it possible to set the switching frequency to 1MHz and use it with an input voltage 5V and an output voltage 1.8V?

Regards,

Masashi