Other Parts Discussed in Thread: UCC21750
Tool/software:
Hi,
I want to use the UCC21750 with an external totem pole buffer to drive a SiC power module (CAB6R0A23GM4T) at 25kHz. In section 9.2.2.8 of the gate driver IC, the following output buffer and external STO circuit are shown:

An RC circuit consisting of Csto and Rsto are used to achieve soft turn-off. The calculation of Rsto is pretty clear from the datasheet, but I need help with the calculation of Csto.

To calculate Csto, the soft turn-off time Tsto must be known. How do I determine or calculate this value for my application? (Note: Vdd = 15V, Vee = -4V)
Also, I would like to understand why the OUTH and OUTL gate driver pins are tied together? By not tying them together, the Rsto resistor can be eliminated. I don't know if I'm missing something, but I can't really think of a reason why tying the two would be beneficial.