Other Parts Discussed in Thread: BQ25622
Tool/software:
Hallo,
Is it possible to receive design files of the BQ25622EVM please?
I would like to check the routing for the device
Thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hallo,
Is it possible to receive design files of the BQ25622EVM please?
I would like to check the routing for the device
Thank you,
Hi,
Using TS_BIAS may save some power. Please see below.
8.3.5.4.5 TS_BIAS Pin (BQ25622 Only)
The The BQ25622 has the TS_BIAS pin to isolate the battery temperature sensing thermistor and associated resistor-divider from REGN. The 103AT thermistor with typical resistor-divider network requires about 400 μA to bias. The BQ25622 provides the TS_BIAS pin, which is internally connected to the REGN LDO via a back-toback MOSFET switch. When no temperature measurement is being taken, the switch is disabled to disconnect the thermistor and resistor-divider from the REGN LDO, saving the 400-μA bias current from being expended unnecessarily. The TS_BIAS pin has short-circuit protection. If a short is detected on the TS_BIAS pin, the switch is disabled to disconnect the short from REGN. If this condition occurs, TS_STAT register is set to 0x3. Charging and OTG modes are suspended until the short is removed.
Thanks,
Ning