Tool/software:
In our application we are using the BQ25792 along with a 3S2P battery. Sometimes the battery can be discharged to a point where the measured voltage (by the BQ chip) is 2.0 volts. Is there a mechanism within the BQ25792 that prevents the battery from discharging (and therefore killing power to the system) if it drops below a certain voltage? In other words is there any sort of low voltage disconnect. I have set VSYSMIN to 9.0 volts.
Kind regards,
Paul