Part Number: TPSM365R3
Tool/software:
I have a circuit designed using the Webench tool. 14.5V input, 6.5V output at 200 mA operating up to 70C ambient using the TPSM365R3R (not FR) device. The details are in the attached PDF generated by the tool.

Recently, due to devices that don't seem to provide that expected efficiency or output voltage under load, my attention has been drawn to a related post for this part:
So my first question is: Was the webench updated per the issues raised in this post (as it appears to be generating the same model as when I first designed this circuit 18 months ago)?
Secondly, my attention was also drawn to Table 9-6 of the datasheet. This seems to suggest that accepting the 1 MHz default frequency from the Webench may be insufficient for reliable operation of the part.

So my second question is: Do I need to increase the frequency (say to 1.2 or 1.4 MHz) to increase my reliability?
Lastly, I would ask: Is there a better tool (than this table or the Webench output) or available formula for estimating the best case operating frequency and efficiency?