Part Number: LM3410
Tool/software:
I am using the LM3410 boost LED driver in my UV LED module and encountered an issue when powering it from a system charger IC.
System setup:
Charger IC: MPS MP2733GQC (NVDC power path charger, Monolithic Power Systems).
Driver IC: LM3410X boost LED driver.
Inductor: AOTA-B252010S100MT (10 µH).
Power source: 5 V adapter.
Battery: single-cell Li-ion.
Issue observed:
When the LM3410 VIN is connected to the MP2733 VSYS pin, the inductor overheats and fails within a few seconds.
Both circuits (MP2733 charger and LM3410 boost LED driver) operate normally when tested independently.
Failure only occurs when the modules are connected in this configuration.
My questions:
Is the LM3410 sensitive to input source impedance or supply regulation behavior (e.g., VSYS of MP2733 is not a raw battery rail but a regulated system output)?
Would you recommend powering LM3410 directly from the battery node (VBATT) instead of VSYS to avoid inductor overstress?
Do you have guidelines or reference designs showing LM3410 driven from a charger’s system rail?