BQ25100: BQ25100 issue

Part Number: BQ25100


Tool/software:

Dear expert:

At present, an abnormal output voltage (-0.005V) of an IC chip was found. After replacing the IC, the output (4.25V) was normal. After cross-verification, it was confirmed that the abnormal output of the IC chip was the cause. Then, the pin performance between the abnormal IC was measured. Confirm that the internal circuit connectivity of the chip is normal (the following data). The voltage output failure cannot be identified as the root cause. We need the manufacturer's assistance to conduct a failure analysis of the IC chip

引脚

阻抗

连通性

1-1

0.585V

正常

1-2

0.455V

正常

1-3

0.457V

正常

2-1

0.451V

正常

2-2

0.604V

正常

2-3

0.604V

正常