This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51388: Simulation request

Part Number: TPS51388


Tool/software:

Hello team,

I have been trying to simulate TPS51388/885 using PSpice but load transient simulation is unable in my environment. Could you simulate based on customer's request instead of me?

Followings are the conditions for load transient simulation. Slew rate is 2.5A/us. If the Cout isn't enough to meet Vout requirement, please add Cout and simulate. Then, please share the image with me.

Device Vin Vout Iout Cout L Fsw Rtop Rbot
1 TPS513885 18V 5.15V±4% 0A<-->10A 33uF 1.5uH 560kHz - -
2 TPS51388 18V 5.0V±4% 0A<-->10A 33uF 1.5uF 600kHz 154kohm 21kohm
3 TPS51388 18V 3.3V±4% 0A<-->10A 53uF 1.0uF 600kHz 154kohm 34kohm
4 TPS51388 18V 1.8V±3% 0A<-->10A 86uF 0.68uF 600kHz 154kohm 76.8kohm

Best regards
koyo