Part Number: TPS62992-Q1
Tool/software:
I was hoping to use the TPS62992-Q1 in alkaline cell powered device that needs to last a year or more between battery swaps. The device wakes up every hour for a minute of so but draws <1uA between wakes. The TPS device's 4uA quiescent operating current was the lowest I could find for a step-down that could handle the 4-cell max voltage of 6.6V. The problem I have discovered is that the TPS62992-Q1 quiescent current rises to over 1mA while in dropout! My circuit has no problem operating at lower voltages so I would like to run the batteries into the ground, but if the TPS62992-Q1 Iq rises to 1mA that will kill the cells in weeks or less when the pack voltage falls to 5V. I'd like to find a part with no Iq rise in dropout but this seems to be rarely (maybe never?) spec'd. I'm a bit surprised that dropout Iq rise is not mentioned more with so many battery powered devices being made.