Part Number: LM5176
Tool/software:
HI team ,
Issue Summary – LM5176-Q1 Buck-Boost Humming Near VIN ≈ VOUT
We are using LM5176-Q1 in a 4-switch buck-boost design, generating 28 V output from a 10–30 V input range.,Vout is set for 28V.
-
V1.0 board: Works fine across the full range, clean SW node, no audible issues.
-
V1.1 board: Same schematic,additional some components placed for EMI/EMC Complaince.
-
Symptom: At VIN = 23–30 V (≈ VOUT), SW node shows burst/noisy behavior (~180 kHz packets) and audible hum. Below 23 V (boost mode) operation is clean.
The issue occurs with no load and with load(Tested with 1.6A). Request your support/analysis to debug the issue .I have attached schematics V1.1 & V1.0 along with waveform capture.LM5176_Buck_Boost_Humming_Noise_Texas_Insturments_V0.1.pdf