Tool/software:
Hello Support,
We use 2 TPS63020QDSJTQ1 for 3v3 and 5v power. Our no load current is 15mA@5V for 2 TPS63020QDSJTQ1. Is it normal or something wrong with our design? Please advise. Thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello Support,
We use 2 TPS63020QDSJTQ1 for 3v3 and 5v power. Our no load current is 15mA@5V for 2 TPS63020QDSJTQ1. Is it normal or something wrong with our design? Please advise. Thanks in advance
Hello Lei,
Please see attached sch.TPS63020QDSJTQ1-NoloadCurrentProblem.pdf
We have 2 tps63020 and when we remove one of them current reduces to 8 mA. We removed inductors(L1 and L2) but still we have 15 mA.
Hi Ibrahim,
Where the 15mA is measured? Is it flow into the VIN pin?
I don't think there will 15mA Iin when there is no load. So further check is needed.
Regards
Lei