Hi
Input: 12V
Output:12V
Issue: The output cannot start up when the load exceeds 12V / 0.6A.
Even after removing the output capacitor, the issue remains.
It seems protection is triggered during startup current.
Is it correct that the circuit cannot operate when power is applied with a load connected?
I’ve already modified components related to inrush current and ILIM, but the output still cannot operate properly above 0.6A.
Thanks