DRV8328: unused nFAULT pin and LSS Pin

Part Number: DRV8328


Hi Team,

I'm not planning to use nFAULT pin and low side current sensing, can nFAULT pin left floating or must it connect to a power source? Can I tie it to the GVDD via 10K or 100K?

As for LSS, if low side current sensing is not used, can it be tied directly to the GND? Since MP6530/1 can do that as well and I think DRV8328 is the pin-to-pin compatible device? (VDSLVL is disabled as well)